Stabiloy cables with Altistart Soft starts
Issue:
Can you use Stabiloy?

Product Line:
Altistart Soft starts

Environment:
All

Cause:
Stabiloy is an Aluminum/Copper Hybrid

Resolution:
Per the Installation Manual, Only Copper Cables are compatible with Schneider Electric Soft start terminals.  Can use Stabiloy only on the high hp range that require lugs.  You will, however, have to use Stabiloy compatible lugs to use those cables.
Aug 2014, Per US Engineering.

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: