{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.

Buscar Preguntas Frecuentes

What is the replacement for the KA frame, I-Line mount breakers?

Article available in these languages: Spanish

Issue:
Replacement for KA36100, KA36125, KA36150, KA36175, KA36200, KA36225 and KA36250 breakers

Product Line:
Obsolete KA frame, I-Line Circuit breakers, except for HCN interiors

Environment:
Products sold in North America

Resolution:
The suggested replacement breaker are:
KA36100 = HGA36100
KA36125 = HGA36125
KA36150 = JGA36150
KA36175 = JGA36175
KA36200 = JGA36200
KA36225 = JGA36225
KA36250 = JGA36250

Breakers are rated 18kA at 600V, 35kA at 480V and 65kA at 240V.  Please note that Powerpact H and J frame breakers are functional equivalent breakers and use the same 4.5 inches of mounting height .

NOTE:
Due to the difference in breaker length from the Legacy breaker to the Powerpact, the mounting foot screw (retaining screw) treads into a different opening than the older circuit breakers. This is designed in this manner, and the panelboard with breakers, has been tested. The purpose of the retaining screw is to keep the breaker from being pulled away from the bus. When the installation is complete, with the breaker in place and the panelboard deadfront trim installed, the breaker will be properly mounted as designed.

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: