{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
Can you program Powerlink NF3000G3 controller via the webpages?
Issue:
Can you program Powerlink NF3000G3 controller via the webpages?

Product Line:
Powerlink G3 Lighting Control

Environment:
Commercial Building, North America
integrated webpage of the NF3000G3 Powerlink Controller

Resolution:
The webpages in NF3000G3 controller are primarily used for Monitoring and Control.  With Monitoring, one can view status of Breakers, Zone, and Inputs.  On the Control page, one can override Breakers, Zones, or Inputs.   The webpage has a Setup Page, this page can be used to program or make changes to the programming.  One uses the mouse to push the buttons and operate the controller as if one were actually working the controller menu screens by hand.

The programming pages of LCSBASIC or LCSADVANCED software are much easier and more intuitive than programming via the controller menus.   The integrated webpages are not a strong substitute for the LCS software.

Schneider Electric Mexico

Explora más
Producto:
Artículos que pueden ser útiles
Explora más
Producto: