{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
What are some of the less common busway plug-in unit catalog number suffixes and their meaning?
Issue:
Product Features, Selection

Product Line:
Busway

Environment:
UL 857, CSA C22.2 No. 27-1973, NFPA 70 Art. 368

Cause:
In order to determine if a busway plug-in unit with few or no additional catalog number suffixes may be a suitable substitution for one which has one or more additional suffixes, the meaning of each suffix must be understood.

Resolution:
Here is a (partial) list of some less common busway plug-in unit catalog number suffixes, and their meaning:

A:     The letter "A" as a suffix designates special lugs, most often understood to be copper compression lugs, unless otherwise specified by the customer.

C:     The letter "C" as a suffix designates copper mechanical lugs.

G:     A single letter "G" as a suffix commonly designates a ground provision on the plug-in unit, and this is now a standard feature, although in the past it was an option.  Where this provision is not desirable (for some older busway installations), this provision is removable.  A second letter "G" suffix in the catalog number is a "partial" suffix:  see "GS", below.

GS:  The letters "GS" as a suffix designate gasketing on the plug-in unit.

LP:  The "LP" suffix denotes "Lug Pad Only" - No Lugs provided on the load base. Customer supplies their own lugs.

R:     The letter "R" as a suffix for a fusible plug-in unit catalog number designates Class R fuse clips.

Schneider Electric Mexico

Explora más
Categoría:
Artículos que pueden ser útiles
Explora más
Categoría: