{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
What type of breakers will install in an NQ panelboard?
Issue:
What type of breakers does an NQ panelboard accept?

Product Line:
NQ

Environment:
Panelboards

Cause:
Need to know what type of breakers can be used in a panelboard

Resolution:
NQ panelboards accept QO and QOB branch breakers. These mount directly to the bus; no additional hardware is required. See individual panelboards for amperage restrictions. Tandem breakers cannot be used in an NQ panelboard.

A subfeed Q-frame, H-frame, or J-frame breaker can also be installed. These require a subfeed breaker kit and a larger enclosure.

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: