What are the clearances required for installation of a QED Switchboard?
Issue:
For the installation of a QED Switchboard what clearances are required?

Product Line:
QED Switchboards

Environment:
Installation

Cause:
Layout clearances

Resolution:
The  INSTALLATION OF SWITCHBOARDS Bulletin Page 8 attached below,  shows clearances definition as:

4.2.1 Clearance from Walls
Clearance from walls (not rear accessible)—minimum of 1/2 inch
4.2.2 Working Clearances
Working clearances vary substantially depending on voltage and specific applications. See Section 110.26 of the National Electrical Code.

Schneider Electric Mexico

Documentos adjuntos
QED Installation guide PB2.1-2007.pdf [201.18 KB]
Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: