Can an I-Line panel be built with Motor Circuit Protectors ?
Issue:
Can MCPs be used in an ILine panel or I-Line distribution in a switchboard?

Product Line:
Panelboards

Environment:
I-Line

Resolution:
No. Factory assembled I-Line panels w/ MCPs are not available. That would violate the NEC code, since the overload protection is not in the same enclosure. This also applies to I-Line distribution in switchboard construction.  I-Line motor circuit protectors are available, but are only used for OEM panels where overload protection is included, for example, in an overload relay block.

Schneider Electric Mexico

Explora más
Rango:
Categoría:
Artículos que pueden ser útiles
Explora más
Rango:
Categoría: