Do we offer Mini Power-Zone Transformers in a NEMA 4X enclosure?

Issue:
Does the suffix SS on an MPZ indicate a Nema 4X stainless steel enclosure?

Product Line:
Mini Power-Zone Transformers

Environment:
Low Voltage Transformers

Cause:
Enclosure Nema Rating

Resolution:
No. While we do offer Mini Power-Zone transformers in standard #304 stainless steel enclosure (suffix SS) or as a special quote in #316 stainless steel enclosure (suffix S6), it is still a NEMA 3R rated enclosure. Either Stainless Steel Mini Power Zone products will be painted ANSI 49 Grey.  We do not offer a NEMA 4X rated enclosure for the Mini Power-Zone product line.

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: