How many HQO Load centers can I install in an I Line panelboard? Is there a limit ?
Issue:
How many HQO Load centers can I install in an I Line panelboard? Is there a limit ?

Product Line:
I Line panelboard and accessories

Environment:
Application

Cause:
Clarification

Resolution:
There is a maximum of HQO distribution load centers allowed which = 7 . Since there are a max of 6, 1 pole spaces per load center, the maximum amount of QO Branch breakers that could be added would = 42 .  This is due to the solid neutral not being able to support more than that.


Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: