Buscar Preguntas Frecuentes
Can the SDSA1175 or SDSA1175T be mounted upside down to the bottom of a NEMA 3R box?
Product Line:
Surge Protective Devices (SPDs)
Environment:
SDSA1175, SDSA1175T
Resolution:
The device can be mounted on the bottom of a NEMA 3R box but the SPD status indicator will be pointed at the ground. To determine a suitable location for mounting the SDSA1175(T), consider the following:
Surge Protective Devices (SPDs)
Environment:
SDSA1175, SDSA1175T
Resolution:
The device can be mounted on the bottom of a NEMA 3R box but the SPD status indicator will be pointed at the ground. To determine a suitable location for mounting the SDSA1175(T), consider the following:
- Free space for mounting the SDSA1175(T) device.
- Use the shortest distance from the mounting space to the required circuit breaker to minimize lead length.
- Convenience of this location to check status LED of the SDSA device.
Publicado para:Schneider Electric Mexico
Explora más
Rango:
Explora más
Rango: