{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
Does Schneider offer DC rated Panelboards?

Article available in these languages: Spanish

Issue:
Panelboard for DC rated applications

Product Line:
NQ NF I-Line Panelboards

Environment:
Products sold in North America

Resolution:
Only the NQ and I-line panels are rated for DC, due to the DC rated breakers that can be installed in them.
NQ panels use QO/QOB breakers which are rated up to 48VDC.  I-Line breakers can be rated up to 250VDC max.
For DC applications using I-Line Panelboards, the amperage range availability is small, 15A-250A maximum using Powerpact H and J frame breakers .

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: