Is the ATV31 drive compatible with Somove software?
Issue:
ATV31 drive compatibility with Somove.

Product Line:
Altivar 31

Environment:
All

Cause:
Software

Resolution:
Yes,  the ATV31 drives can be used with Somove software.
The DTM files for altivar drives will need to be installed as seen from link below.

DTM file for all other supported Altivar series drives:
https://www.se.com/ww/en/download/document/Altivar_DTM_Library

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: