Is there an 80 Degrees C temperature rise version of the 9070T1500D24?

Issue:
Is there an 80 Degrees C temperature rise version of the 9070T1500D24?

Product Line:
9070T Control Power Transformers (CPT)

Environment:
Application

Cause:
Environment

Answer:
Only 200-300VA 9070T transformers have a 80 DEG C rise rating , 115 DEG C is minimum offering for 1200VA and up

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: