How to correct error 22321 Liquid:Calculation of Density at base conditions unsuccessful in Realflo?
Scenario:
  • The scadapack is polling values from the Coriolis Meter.
  • When the Coriolis Meter losses connections or it stop communicating, The Realflo Run liquid will use the default setting parameters.
  • Make sure that correct parameters are entered on the Default value.
For example: If the default value for the Density was set to 1 when measuring Liquid and the Coriolis meter losses communications then
the flow computer will used the default value 1 to calculate the flow and will give an error result of 22321 "Liquid:Calculation of Density at base conditions unsuccessful"

Use the table below for Density default value:

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: