Is there any potential Trio ER450 radio interference between Microwave antenna?
Typically there is NO concern of interference between a 450 MHz system and a microwave system, as microwave is above 3000 MHz. (3 GHz)
Such great frequency separation gives a lot of isolation for interference. I would still recommend the new dish be installed a 2 meter or
more away from the 450 MHz antenna, to minimize any minor interference concern. Also, if closer the metal of the dish might affect
the radiation pattern of the 450 MHz antenna.

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: