Does any of SCADAPack 4000 series transmitters require secondary seal?
All SCADAPack 4000 series transmitters (Models 4012, 4032, 4102, 4103, 4202 and 4203) meet the requirements of “Second Seal Compliance” for the Canadian Electrical Code.

SCADAPack 4000 series products have had approvals and markings for ANSI/ISA 12.27.01 Single Seal Compliance since May 2008.
This approval meets the requirements of the CEC for installation without additional secondary seals on the electrical connections for all products up to 3000 psi MWP.

Schneider Electric Mexico

Documentos adjuntos
Single Seal Compliance - SCADASense .pdf [188.34 KB]
Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: