Buscar Preguntas Frecuentes
What are the standard features of the Surgelogic Surgloc SPDs?
Issue:
Identify the standard features of the Surgelogic Surgloc SPDs
Product Line:
Surge Protective Devices (SPDs)
Environment:
Surge Protection and Power Conditioning
Resolution:
The standard features are as follows;
Identify the standard features of the Surgelogic Surgloc SPDs
Product Line:
Surge Protective Devices (SPDs)
Environment:
Surge Protection and Power Conditioning
Resolution:
The standard features are as follows;
- 10 year warranty
- 10 modes of protection
- NQ retrofit for existing NQ panels
- 200KA SCCR
- Counter and Dry contacts
- Audible alarm with enable and disable switch
- LED indicators, green (normal) and red (fault indicators) for each phase
Publicado para:Schneider Electric Mexico
Explora más
Rango:
Explora más
Rango: