What would cause the ATV600 or ATV900 to show Run 0.0hz if I'm not using anything external to adjust the speed?
Issue:
What would cause the ATV630 to show Run 0.0hz if I'm not using anything external to adjust the speed?

Product Line:
ATV630

Environment:
All


Cause:
Programming


Resolution:

If you're not using an external speed reference (i.e. Potentiometer, Transducer, etc.), when you close 24v to DI1 the drive shows 0.0hz.  You will need to go to [Simply Start] set [Low Speed] to 60hz (or desired speed)

Schneider Electric Mexico

Explora más
Rango:
Categoría:
Artículos que pueden ser útiles
Explora más
Rango:
Categoría: