{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
Can the HJKADAPT adapter plate be used to go from an FA/FH or KA/KH to a B-frame breaker?
Issue:
What is the adapter kit for B frame to be use as alternative for the unit mounted FA or KA frame breakers?

Product Line:
Circuit Breakers

Resolution:
When replacing a unit mounted FA/FH or KA/KH breaker, adapter plate HJKADAPT was used to allow a Powerpact B frame breaker to be used as the replacement. Note that the HJKADAPT kit is NOT intended for use in Square D circuit breaker enclosures or with a remote operator however, HJKADAPT is already obsolete without replacement. Field services need to be contacted if replacement is needed.

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: