Buscar Preguntas Frecuentes
Are fuses supplied with the class 8998 fusible branch feeder units for Model 4 MCC's?
Issue:
Do Model 4 MCC's come with the fuses installed?
Product Line:
Model 4 Motor Control Centers
Environment:
Class 8998 Branch Feeder Units for Model 4 Motor Control Centers
Resolution:
No, the Class 8998 fusible branch feeder units do not come with fuses. Fuses need to be purchased separately. Class H or Class R fuses can be used with fuse clips.
Do Model 4 MCC's come with the fuses installed?
Product Line:
Model 4 Motor Control Centers
Environment:
Class 8998 Branch Feeder Units for Model 4 Motor Control Centers
Resolution:
No, the Class 8998 fusible branch feeder units do not come with fuses. Fuses need to be purchased separately. Class H or Class R fuses can be used with fuse clips.
Publicado para:Schneider Electric Mexico
Explora más
Categoría:
Explora más
Categoría: