Is the TC2931-204 Changeover Thermostat, Strap-On, Summer/Winter type still available?
Issue:
Is the 10 foot cabled version TC2931-204 Changeover Thermostat, Strap-On, Summer/Winter type still available?

Product Line:
Thermostats

Environment:
Application

Cause:
Avialability

Resolution:
The TC-2931-204 Thermostat with 10 ft. (3 m) cable and plug (which cannot be extended) for unit ventilator, is Obsolete/NLA
The TC-2931 comes with std 3 ft cable leads , (which cannot be extended)
The TC-2931-205 comes with 3 ft. (914 mm) cable (which cannot be extended)  used with CP-5341 Drive

Schneider Electric Mexico

Documentos adjuntos
TC-2931 - TC-2942 F-12720.pdf [54.89 KB]
Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: