Can the Altivar 340 programming be saved to the VW3A1111 Keypad?
Issue:
ATV340 saving parameters to the Keypad VW3A1111.

Product Line:
Altivar 340

Environment:
All

Cause:
Configuration

Resolution:
Yes, the ATV340 works the same way as the ATV630 and ATV930.  Browse to [Main Menu] > [File Management] > [Transfer Config File] > select "Copy from the drive" to backup to the keypad.

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: