What are the differences in NEMA enclosure ratings, types?

Article available in these languages: Spanish

Issue:
Where is a Table with Nema enclosure ratings definitions?

Product Line:
Enclosures

Environment:
Application

Cause:
Degrees of Protection for enclosures

Resolution:
Definition descriptions are below:

NEMA 1 enclosures are typically used for protecting controls and terminations from objects and personnel. This style of enclosure, while offering a latching door, does not have a gasketed sealing surface. NEMA 1 enclosures are used in applications where sealing out dust, oil, and water is not required.

NEMA 2 enclosures are intended for indoor use primarily to provide a degree of protection against limited amounts of falling water and dirt. NEMA 3 enclosures are intended for outdoor use primarily to provide a degree of protection against windblown dust, rain, sleet, and external ice formation.

NEMA 3R enclosures are typically used in outdoor applications for wiring and junction boxes. This style of enclosure provides protection against falling rain, sleet, snow, and external ice formation. Indoors they protect against dripping water. This style of enclosure does not have a gasketed sealing surface. Some models have hasps for padlocking.

NEMA 3S enclosures are intended for outdoor use primarily to provide a degree of protection against windblown dust, rain, sleet, and to provide for operation of external mechanisms when ice laden.

NEMA 4 enclosures are gasketed and the door is clamped for maximum sealing. NEMA 4 enclosures are used in many applications where an occasional washdown occurs or where machine tool cutter coolant is used. They also serve in applications where a pressurized stream of water will be used.

NEMA 4X enclosures are made of stainless steel, aluminum, fiberglass, or polycarbonate. NEMA 4X enclosures are used in harsh environments where corrosive materials and caustic cleaners are used. Applications include food, such as meat/poultry processing facilities, where total washdown with disinfectants occur repeatedly, and petro-chemical facilities, including offshore petroleum sites.

NEMA 5 enclosures are intended for indoor use primarily to provide a degree of protection against settling airborne dust, falling dirt, and dripping non-corrosive liquids.

NEMA 6 enclosures are intended for indoor or outdoor use primarily to provide a degree of protection against the entry of water during occasional, temporary submersion at a limited depth.

NEMA 6P enclosures are intended for indoor or outdoor use primarily to provide a degree of protection against the entry of water during prolonged submersion at a limited depth.

NEMA 11 enclosures are intended for indoor use primarily to provide, by oil submersion, a degree of protection to enclosed equipment against the corrosive effects of liquids and gases.

NEMA 12 enclosures are intended for indoor use to provide a degree of protection against drips, falling dirt, and dripping non-corrosive liquids. NEMA 12 enclosures are most commonly used for indoor applications of automation control and electronic drives systems, including packaging, material handling, non-corrosive process control, and manufacturing applications. Gasketed doors seal the enclosure’s contents from airborne contaminants and non-pressurized water and oil.

NEMA 12K enclosures with knock-outs are intended for indoor use primarily to provide a degree of protection against dust, falling dirt, and dripping non-corrosive liquids other than at knock-outs.

NEMA 13 enclosures are intended for indoor use primarily to provide a degree of protection against dust, spraying of water, oil, and non-corrosive coolant.

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: