Can we adjust the overload relay while the motor is running?

Issue:
Customer wants to adjust the LR9F overload while the motor is running.

Product line:
LRD, LR9, LR9F, 9065 solid state, SSOLR

Environment:
All solid state or overloads with adjustable dials.

Resolution:
It is recommended to stop the motor and then adjust the overload settings.

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: