{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
What is the replacement actuator for an EM42?
Issue:
Can a replacement EM42 actuator be bought here in the United States ?

Product Line:
European Actuators

Environment:
Maintenance

Cause:
Replacement

Resolution:
The EM42 Actuator is a European type and not available here in the USA . It is also obsolete and crossed to a M310 actuator which is also obsolete.
Current functional replacement actuator  is a M400 actuator. It is recommended to check existing valve specification so a correct replacement can be advised.

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: