What is the packing kit for a VB-9213-000-4 valve if the pipe size isn't known?

Issue:
What is the packing kit for a 1/2 " to 2" VB-9XXX Series valve?

Product Line:
Valves and Actuators

Environment:
Maintenance

Cause:
Replacement

Resolution:
Since there is a "4" in the valve part number VB-9213-000-4-XX for NPT connection, the valve sizes would have to be 1/2" to 2". That would make this valve the obsoleted VB-9XXX Series.
After the 2" NPT valves comes the 2 1/2"- 6" Flange valves with a "5" where the "4" used to be.
The rebuild packing kit YBA-635, is for the obsoleted VB-9XXX series 1/2 "-2" valves

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: