Buscar Preguntas Frecuentes
What is the difference between the MA-5213 actuator and MP-5213 Actuator ?
Issue:
What is the difference between MA and MP actuators?
Product Line:
Valves and Actuators
Environment:
Application
Cause:
Product Features
Resolution:
The Specifications for each Actuator below shows the MAJOR difference between the 2 actuators is that the MP actuator is Proportionally controlled , whereas the MA actuator is a 2 position On/Off.
Actuator: (MP-5213): What is the difference between MA and MP actuators?
Product Line:
Valves and Actuators
Environment:
Application
Cause:
Product Features
Resolution:
The Specifications for each Actuator below shows the MAJOR difference between the 2 actuators is that the MP actuator is Proportionally controlled , whereas the MA actuator is a 2 position On/Off.
- Actuator Type: Electric/Hydraulic
- Control Signal: Proportional
- Control Signal Range: 6 to 9 VDC
- Loss of Power Type: Spring Return
- Power Input Voltage: 24 VAC
- Leads and Connections: 4 ft Appliance
- Torque: 1.86 in-lb
- Mechanical Movement: Linear
- Protection Rating: NEMA 1
- Product Line: Schneider Electric
- Product Range: Electronic Hydraulic
Actuator: (MA-5213):
- Actuator Type: Electric/Hydraulic
- Control Signal: 2-Position (On/Off)
- Loss of Power Type: Spring Return
- Power Input Voltage: 24 VAC
- Leads and Connections: 4 ft Appliance
- Torque: 20 in-lb
- Mechanical Movement: Linear
- Protection Rating: NEMA 1
- Product Line: Schneider Electric
- Product Range: Electronic Hydraulic
Publicado para:Schneider Electric Mexico
Explora más
Rango:
Explora más
Rango: