What is "SSC" setting on the ATS22 Softstarter?

Issue:
Recommendation for SSC setting on ATS22 Softstarter.

Product Line:
Altistart 22, ATS22

Environment:
All serial numbers

Cause:
On a new installation, should it be On or Off?

Resolution:
Default is "On"  which means that Acceleration (ACC) and Deceleration (DEC) are controlled by torque.
When SSC=On the soft starter will set automatically the Start-stop profile control voltage.
This configuration is suitable for most of the applications, and especially pumps.

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: