{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.

Buscar Preguntas Frecuentes

Is the Telefast ABE-7H16S43 compatible with the BMXDDI3202K and BMXDDI6402K modules?

Issue
Beginning with the 2019 catalog, it states that the modules are not compatible. The older catalogs, user guides and programming versions stated that it was. The latest version of Control Expert and the latest Modicon X80 Discrete I/O user manual both have been updated to indicate the incompatibility.

Product line
Telefast, Control Expert, Modicon X80

Resolution
It was discovered that there’s incompatibility between the X80 DI modules (BMXDDI3202K/6402K) and ABE7H16S43. The leakage current through the red LED (blown fuse indicator) is greater than the threshold current of X80 DI modules and through this path the voltage applied to DI module’s port is greater than the threshold as well. The modules are not compatible.

The following can be used:

Connection bases ->  ABE-7H08R**, ABE-7H08S21, ABE-7H16R**, ABE-7H16S21, ABE-7H16R23

Input adapter connection bases -> ABE-7S16E2** and ABE-7P16F3**

Schneider Electric Mexico

Explora más
Producto:
Rango:
Explora más
Producto:
Rango: