What is the difference between a MN-S3HT-500 and MN-S3HT-500-A sensor?
Issue:
How can you order Made, or assembled in America MN-S3XX-500 sensors ?

Product:
Sensors

Environment:
Application

Cause:
Product Features

Resolution:
The only difference between the MN-S3HT-500 and MN-S3HT-500-A Sensor , is the MN-S3HT-500-A indicates the Sensor is labeled "Made in America"vsMN-S3HT-500 Sensor which labeled "Made in China"

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: