{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
What is the cross for a MA-407-701-0-4 actuator ?
Issue:
Is there a replacement for the MA-407-701 actuator?

Product:
Valves and Actuators

Environment:
Maintenance

Cause:
Replacement

Resolution:
The MA-407-701-0-4 is an OEM actuator which crosses to a MA-407-701 actuator could use 120vac or 240vac , with a factory preset rotation of 113 deg. Both Actuators are obsolete and not available, but a MA-418-500 120VAC actuator, or the  MA-419-500 240VAC actuator can be used to replace it.  Rotation from the Factory is 170 deg for the MA-418, and MA-419 actuators, and would need to be field adjusted to 113 deg for an equal cross.

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: