{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
What is the programming software for the TM221 processors?
Issue
SoMachine does not list the TM221 processors, what are they programmed with?

Product line
TM221, SoMachine, SoMachine Basic, EcoStruxure Machine Expert Basic

Resolution
The programming software for the M221 is  EcoStruxure Machine Expert Basic. It is a free download that can be found on www.se.com.
https://www.se.com/us/en/product/ESEBASXZZPA10/ecostruxuremachine-expert-basic-free-licence-programing-software-for-m221-controllers/

This software can be used to program the Modicon M221 line of PLCs and is the successor to SoMachine Basic v1.6 SP2 moving forward. Project files from SoMachine Basic can be automatically migrated to EcoStruxure Machine Expert Basic by simply opening the .smbp extension files in EcoStruxure Machine Expert Basic.

As for a cable, you can use any standard USB to Mini USB cable.

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: