Buscar Preguntas Frecuentes
Will a 4 pole Busway switch plug into 3 Pole Busway?
Issue:
Can Plug in Busway switches be mixed , 3 Pole , or 4 Pole, into 4 , or 3 pole opposite Busway respectively?
Product:
I Line Busplugs
Environment:
Application
Cause:
Product Features
Resolution:
The 4 pole fusible / breaker switches can be installed into 3P Busway. This also works with 3P switches plugging into 4P Busway.
The EXCEPTION is when the BusPlug's p/n starts with "PT". These switches have a Joint pak connection on the back of them, specifically orientated for the same amount of bussing and poles.
They CANNOT be mixed.
Publicado para:Schneider Electric Mexico
Explora más
Rango:
Explora más
Rango: