What is the Form A11?

Issue:
A11 Form description with motor starters

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
NEMA Contactors and Starters

Resolution:
Addition of single black push button, with contact block, 9001KA1, markings to be specified. Unwired unless wire diagram is supplied.
This also applies to all 8536, 8538, 8539, 8606, 8630, 8640, 8702, 8736, 8738, 8739, 8810, 8903, 8940, 8941, and 8941 devices.

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: