{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.

Buscar Preguntas Frecuentes

Are the fuse clips replaceable on I Line Busplugs?

Issue:
Can Fuse clips and Fuse bases be replaced in I I-line bus plugs?
Product Line:
Busway
Environment:
Bus plugs

Cause:
Maintenance and replacement parts are often needed and being able to get fuse clips and fuse base replacements for I Line Busplugs may become necessary. Knowing the amperage and series is necessary in determining if parts are available

Resolution:
Replacement Load base fuse bases and clips are available for replacement for the following Series Switches :
PQ (30-100A) Series 004
PQ (200A) Series 006
PS (200) Series 005
PBQ (400A & 600A) Series 006

Only the LOAD fuse base assembly is replaceable on this plug-in unit. The line side fuse clips are not field replaceable.


Load Bases for 800A thru 1600A fusible plug-in units are not available
load base
CTA-ID : 2003621

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: