{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
What is a OPF2 fault on a ATV12 drive?

Article available in these languages: Spanish

Issue:
Getting an OPF2 fault on the ATV12

Product Line:
Altivar Machine, ATV12

Environment:
All serial numbers

Cause:
• Motor not connected
• Motor power too low, below 6% of the drive nominal current
• Output contactor open
• Instantaneous instability in the motor current

Resolution:
• Check the connections from the drive to the motor
• Test on a low-power motor or without a motor: In factory settings mode, motor phase loss detection is active Output Phase loss detection OPLpage 94 = YES. To check the drive in a test or maintenance environment, without having to use a motor with the same rating as the drive, deactivate motor phase loss detection Output Phase loss detection OPL = nO
• Check and optimize the following parameters: IR compensation UFr page 58, Rated motor voltageUnS page 57 and Rated motor current nCr page 57 and perform an Auto-tuning tUn page 60

ATV12 user manual:

https://www.se.com/ww/en/download/document/BBV28581/

Schneider Electric Mexico

Documentos adjuntos
ATV12_user_manual_EN_BBV28581_04.pdf [3.62 MB]
Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: