ASCO and Square D SPD Voltage options by Schneider Electric for Surge Protection Devices

Issue:
What are the voltage options / codes for a surge protection device (SPD)

Environment:
Surge Protection

Cause:
Must know the EXACT voltage system that the SPD will be applied to, for example, voltage readings from L-G, L-N, and L-L. If you are not able to provide voltages readings the please specify if the voltage system is a Wye, Delta, High-Leg Delta (HLD), High-Resistance Ground (HRG), Single Phase, or Split-Phase. Please also provide the peak surge current rating that is needed or any other specifications so that we can provide an accurate SPD solution. For example, surge counter, specific enclosure, EMI/RFI filtering, Type 1, Type 2, or integral disconnect switch.

Resolution:
Select the correct voltage code needed for your SPD installation and voltage requirement

SE  / ASCO

Voltage Code


Voltage Description
01    /     120S120/240V 1Ph 3W + G (Split Ph)
02    /    120Y    (Note 1)208Y/120V 3Ph Wye 4W + G
03     /     240H240/120V HLD (Phase B High-Leg)
04    /     277Y    (Note 2)480Y/277V 3Ph Wye 4W + G
05     /    480D    (Note 3)480V DELTA  3Ph Delta 3W + G
06    /    240D 240V DELTA 3Ph Delta 3W + G
08     /    347Y600Y/347V 3Ph Wye 4W + G
09    /     600D    (Note 4)600V DELTA 3Ph Delta 3W + G
12    /    240N    (Note 5)240V 1Ph 2W + G
18    /    240S    (Note 6)480/240V 1P (Split Phase)
11    /    120N    (Note 7)120V 1Ph 2W + G (Split Ph)

1.   208Y/120 series also applies to the following voltage 220Y/127
2.   480Y/277 series also applies to the following voltages 380Y/220, 400Y/230, and 415Y/240
3.   480V Delta series also applies to the following voltage 480Y/277V HRG
4.   600V Delta series also applies to the following voltages 600Y/347V HRG
5.  Only available in the EMB series (EMB72F)
6.  Only available in the EMB series (EMBA2F)
7.  Only available in the EMB series (EMB02F)

Product Line:
ASCO, Square D, and Schneider Electric SPD Surge Protection Device Voltage Code options
HEPD, SDSA, IMA, EMA, EBA  (SSP and TVS and MA), DRSE, HWA, ICSE, IESE, LC, PoESE, QMB, SLACSE, XR, XW
ASCO Series 300, 400 Series
318    331    335    340    350    360    420   425    430    430   440    450    451    452   460  465    480  XDSE  EMA  HWA

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: