Do we offer fire alarm breaker lock offs for QO and/or Homeline breakers?

Issue:
Wants FA lockoffs for QO / Homeline breakers

Product Line:
QO, Homeline breakers

Resolution:
No, there are no special lock offs available for fire alarm breakers as shown below. The code only requires a nameplate identifying fire alarm breakers. The handle or lock off does not have to be red or indicate a fire alarm breaker.

fa lock

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: