Can OFS Server communicate to an M340 via the USB port?
Issue:
OFS server communication to M340 USB port


Product Line:
OFS Server, M340


Resolution:
Yes, OFS Server can communicate to an M340 PLC via the USB port. To configure the OFS server to communicate to the M340 via USB, launch the OFS configuration tool. Then create an alias by selecting "File"  then "New Device Alias". Next click on the ellipsis for Device address 1 to add the USB driver. Select M340 for the Device type and add the symbol table file. Save the configuration

image

Select the USB driver as shown and select ok.
image1

Schneider Electric Mexico

Explora más
Producto:
Artículos que pueden ser útiles
Explora más
Producto: