Product Line:
Powerpact R-frame Circuit Breaker
Environment:
Circuit Breaker
Cause:
Need help decoding "TA" suffix in a Powerpact RKA36120CU31ATA breaker.
Resolution:
The "TA" suffix on the I-Line R-frame means each pole of the load end of the breaker has a bus connector with 3 threaded holes (no bolts or nuts).
Publicado para:Schneider Electric Mexico