Product Line:
QO Load Center
Environment:
Enclosed Molded Case Switch and Enclosed Circuit Breaker Devices
Cause:
What is the difference between the enclosure that comes with the QO200TR and the QO2TR?
Resolution:
The interiors for these two are different. The QO200TR is tested and listed as a molded case switch with no overcurrent protection. It comes with a QO200 factory installed. While the QO2TR is tested and listed as a circuit breaker enclosure in which customer can install a molded case QO circuit breaker. The enclosures may look the same but the interior supplied on both are different. And the interiors for these two are not interchangeable or swapped.
Publicado para:Schneider Electric Mexico