{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.

Buscar Preguntas Frecuentes

I-Line II Busway Tee Catalog Number System

Issue:

How does an I-Line II busway Tee Catalog# is formed?

Product Line:

I-Line II Busways Accessories

Environment:

Products sold in North America

Resolution:

An I-Line II busway prefix should be present first.

The existing busway should be identified so that the catalog# prefix would be available.

For example: AF2516G10ST has a busway suffix of AF2516G as the base of the catalog# which tells us what are the specifications of the busway. The catalog# for the tee can be obtained on "Table 55 - Tees—Dimensions and Catalog No. Suffix" of 5600CT9101 which results to AF2516G-39TFS13B13S13.

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: