Issue:
Enclosure and breaker Ratings
Product Line:
QO Circuit Breaker Enclosures
Resolution:
The current QO Circuit Breaker Enclosure, catalog number CQOE260GFINM Series G02 comes from the factory with a QO260GFI3W breaker installed. This breakers is a 120/240Vac Max. 3 wire breaker that contains the load neutral. But the older Series G, came with a QO260GFI, which did not contain a load neutral connection. If someone has the older Series device with the QO260GFI, the breaker can be changed out in the field with the new breaker QO260GFI3W for 3 wire applications.