Cradle Position Switches for Masterpact MTZ Breaker

Issue:
Adding cradle or breaker position switches to MTZ cradle

Resolution:
If the he cradle does not have any connected, disconnected or test switches. You can add them using:

  • 1a/1b Form C Connected/Test/Disconnected Switch LV833170SP (1 per order)
  • Set of 3 Cell Switch Actuating Arms LV848560SP
  • Push-in Terminal kit (3 Wires) LV847849SP (1 per order)

For more information on these and other signaling options for the Masterpact you may access these catalog pages .

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: