Does Square D Offer a Cover with a door for the small 2-4, 6-12 or 4-8 space Homeline Load Centers?
Issue:
Product design

Product line:
Homeline load centers

Cause:
Application

Resolution:
No. The small Homeline load centers, catalog numbers HOM24L70F or S, HOM612L100F or S, and the HOM48L125C DO NOT contain doors on the covers and there are NO covers with doors available for these small load centers. if a cover with a door is required, consider using the QO type load centers, for example the QO612L100DS or QO816L100DF etc. For additional QO Catalog numbers see the current On-Line Digest pages

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: