{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
ECB24015G3 UL Regulation update

Issue:
Changes to UL Regulation for breaker testing requires update to ECB-G3 15A breaker label and documentation.

Product Line:
ECB-G3 15A one, two, and three pole

Environment:
ECB-G3

Cause:
UL Regulations that took effect in 2022, required a new test on the ECB24015G3 circuit breaker.

Resolution:

New label and documentation stating the 15 A ECB-G3 one, two, and three-pole products should not be used with 14 AWG wire. Use only 12 AWG or larger wire when wiring this device.

The change from 14 AWG to 12 AWG or larger wiring size was necessary for the product to perform adequately during this new test.

Date code: 24114

Note: Anything prior to this date does not require 12 AWG wire.

Schneider Electric Mexico

Explora más
Producto:
Rango:
Explora más
Producto:
Rango: