Issue:
How to field install a rodent barrier or closing plate for an existing QED 2
Product Line:
Switchboards
Environment:
QED, QED2, CMM, Custom switchboards
Cause:
Instructions on how to field install a rodent barrier
Resolution:
Yes, rodent barrier is a field installable option on an existing QED Switchboard. If part numbers are required, please provide FO number of the switchboard to your local distributor and they will contact the local Schneider sales office to work directly with the plant for part numbers and to order. Please see the installation instructions for both N1 and N3R applications below;
NEMA 1: https://www.se.com/us/en/download/document/80230-024-01/
NEMA 3R: https://www.se.com/us/en/download/document/80233-279-03/