Which is the size of the adapter I would need to do an oil sample on a Medium Voltage Transformer?

Issue:

I need to do an oil sample in a three-phase medium voltage transformer and I`m looking to know which is the size of the adapter I would need to connect with the oil pipe.

Product Line:

Medium Voltage Transformers

Environment:

Pad Mounted

Resolution:

The transformer drain valve has a sampling port. The oil sample syringe will have tubes that connect to the port, no adapter is required.

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: