Issue:
The estimated runtime per unit is not in the technical specs, operation manual, or in specifications section of the website.
Product line:
Galaxy VS
Environment:
All models, all serial numbers
Cause:
Galaxy VS runtime tables could be mixed with all the documentation on the website or it is not available on all WW websites.
Resolution:
The runtime tables are available in the Documents Section in the English version Website of the Galaxy VS specific Model. They can be found as Modular Battery Runtime Chart.
The runtime depends on the capacity and the battery strings installed.
Links to Battery Runtimes depending on the UPS Battery Strings
Galaxy VS UPS for up to 2 Internal 7 Ah Modular Battery Strings
Galaxy VS UPS for up to 4 Internal 9 Ah Modular Battery Strings and Modular Battery Cabinets
Galaxy VS UPS for up to 5 Internal 9 Ah Modular Battery Strings and Modular Battery Cabinets