{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is M340 and M580 or Quantum can be installed in SIL1 application?

M340 is not and will not be certified SIL1.
The only range with SIL certification is Quantum. It is certified up to SIL3. So the Quantum family (140cpu67160s, 140cpu65160s) could be used up to sil3 application. M580 is planned to have SIL certification (2017) in future but not with the present offer.

Schneider Electric Malaysia

Explore more
Range:
Modicon QuantumModicon X80 modulesModicon M340Profibus DP FieldbusModicon M580
Explore more
Range:
Modicon QuantumModicon X80 modulesModicon M340Profibus DP FieldbusModicon M580
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.